AXIS#.SAFEPARAM.SOS.RESTARTACKBEHAVIOR

Description

Indicates whether the Safe Operating Stop (SOS) automatically resets or requires a manual reset using safe input or FSoE. In Automatic Restart mode, when the SOS input clears, the SOS automatically restarts (i.e., the function is cleared). In Manual Restart mode, when the SOS input clears, the SOS function remains active until the configured input triggers the SOS to restart. (See AXIS#.SAFEPARAM.SOS.RESTARTACKSOURCE).

Value

Description

0

Automatic restart (Default)

1

Manual restart

 

Context

For complete SOS information refer to SOS (Safe Operating Stop).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Automatic restart)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SOS_1.RESTARTACKBEHAVIOR

315bh

08h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SOS_2.RESTARTACKBEHAVIOR

3172h

08h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SOS_1.RESTARTACKBEHAVIOR

325bh

08h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SOS_2.RESTARTACKBEHAVIOR

3272h

08h

Unsigned8

-

-

Read/Write

No